TGML Rectangle
The <Rectangle> element defines a rectangle. You can create rounded rectangles by setting values for the attributes RadiusX and RadiusY.
| Attribute | Type | Description | 
|---|---|---|
| 
                                                         Fill  | 
                                                    
                                                         Brush  | 
                                                    
                                                         Specifies how the interior of the shape is painted.  | 
                                                
| 
                                                         Height  | 
                                                    
                                                         Double  | 
                                                    
                                                         The height of the rectangle.  | 
                                                
| 
                                                         Left  | 
                                                    
                                                         Double  | 
                                                    
                                                         The x coordinate of the upper left corner of the rectangle.  | 
                                                
| 
                                                         Opacity  | 
                                                    
                                                         Double  | 
                                                    
                                                         A value between "0.0" (transparent) and "1.0" (opaque)  | 
                                                
| 
                                                         RadiusX  | 
                                                    
                                                         Double  | 
                                                    
                                                         For rounded rectangles. The x axis radius of the ellipse used to round off the corners of the rectangle.  | 
                                                
| 
                                                         RadiusY  | 
                                                    
                                                         Double  | 
                                                    
                                                         For rounded rectangles. The y axis radius of the ellipse used to round off the corners of the rectangle.  | 
                                                
| 
                                                         Stroke  | 
                                                    
                                                         Brush  | 
                                                    
                                                         Describes how the line is painted.  | 
                                                
| 
                                                         StrokeDashArray  | 
                                                    
                                                         Array of Double  | 
                                                    
                                                         The pattern of dashes and gaps used to outline shapes:  | 
                                                
| 
                                                         StrokeWidth  | 
                                                    
                                                         Double  | 
                                                    
                                                         The width of the outline of a line.  | 
                                                
| 
                                                         Top  | 
                                                    
                                                         Double  | 
                                                    
                                                         The y coordinate of the upper left corner of the rectangle.  | 
                                                
| Visibility | Visibility | 
                                                         Specifies if the element is visible or not.  | 
                                                
| 
                                                         Width  | 
                                                    
                                                         Double  | 
                                                    
                                                         The width of the rectangle.  | 
                                                
Example:
<TGML>
    <Rectangle Left="10" Top="10" Width="100" Height="50" Fill="#FFFF00" Stroke="#000000"/>
    <Rectangle Left="120" Top="10" Width="100" Height="50" Fill="#FFFF00" Stroke="#000000" RadiusX="10" RadiusY="10"/>
</TGML>
                                            Example on screen: